Min_Current

Min_Current

Address: 4112 (1010H)
Type: WORD
Access: Read/Write
Unit: mA
Range: 0 to Max drive current
Default Value: 0
Store Supported: Yes
Description:

It sets the motor’s reduced current. The drive automatically reduces the current after a current reduction time (Time_RWC object) at the end of the movement

Notes: The current set is the Irms current. The peak current is Irms * 1.4.